i.MX6 trace connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 trace connection

2,382件の閲覧回数
vladislavkasik
Contributor II

Hi,

Is there any application note regarding the ARM trace connection on i.MX6 series for connecting DSTREAM or Lauterbach PowerTrace? None of the demo boards (SABRESDB, SABREAI) count with trace connection, they have only JTAG connector. Does the trace even work on i.MX6? According to the i.MX datasheet the trace signals are available as an alternate function on some pins and the frequency can be up to 600MHz so I assume that there must be some design recommendation.

Thanks,

Vladislav

jiri-b36968

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,535件の閲覧回数
Yuri
NXP Employee
NXP Employee

As for PCB design, You may use recommendations from section 9.4 (PCB guidelines) of “RealView ICE and Trace User Guide”.

http://infocenter.arm.com/help/topic/com.arm.doc.dui0155j/DUI0155J_rvi_user_guide.pdf

0 件の賞賛
返信

1,535件の閲覧回数
jiri-b36968
NXP Employee
NXP Employee

Hi Vladislav,

yes trace it of course possible. There are two ways. You can use Embedded Trace Buffer (16kB) and access it via JTAG. Or you can use Trace port interface and up to 16 bits trace lines (pins alt function in IOMUX). So you can use Lauterbach of DSTREAM for trace to their bigger buffers.

/Jiri

0 件の賞賛
返信