i.MX6 trace connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 trace connection

1,867 Views
vladislavkasik
Contributor II

Hi,

Is there any application note regarding the ARM trace connection on i.MX6 series for connecting DSTREAM or Lauterbach PowerTrace? None of the demo boards (SABRESDB, SABREAI) count with trace connection, they have only JTAG connector. Does the trace even work on i.MX6? According to the i.MX datasheet the trace signals are available as an alternate function on some pins and the frequency can be up to 600MHz so I assume that there must be some design recommendation.

Thanks,

Vladislav

jiri-b36968

Labels (1)
0 Kudos
Reply
2 Replies

1,020 Views
Yuri
NXP Employee
NXP Employee

As for PCB design, You may use recommendations from section 9.4 (PCB guidelines) of “RealView ICE and Trace User Guide”.

http://infocenter.arm.com/help/topic/com.arm.doc.dui0155j/DUI0155J_rvi_user_guide.pdf

0 Kudos
Reply

1,020 Views
jiri-b36968
NXP Employee
NXP Employee

Hi Vladislav,

yes trace it of course possible. There are two ways. You can use Embedded Trace Buffer (16kB) and access it via JTAG. Or you can use Trace port interface and up to 16 bits trace lines (pins alt function in IOMUX). So you can use Lauterbach of DSTREAM for trace to their bigger buffers.

/Jiri

0 Kudos
Reply