i.MX6 sololite parallel camera specifications

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 sololite parallel camera specifications

ソリューションへジャンプ
1,967件の閲覧回数
JHY
Contributor IV

I have a question about CSI camera parallel interface.

I want to know specifications or limitation of CSI of i.MX6 sololite.

Please let me know where the reference webs or documets are.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,614件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please refer to Chapter 16 [CMOS Sensor Interface (CSI)] of the i.MX6 SL Reference Manual.

In particular - sections  16.1 (Overview) and 16.4 (Principles of Operation).

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SLRM.pdf


As for hardware specs, please the i.MX6 SL Datasheet, section 4.10.2
[CMOS Sensor Interface (CSI) Timing Parameters]

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SLCEC.pdf

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,615件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please refer to Chapter 16 [CMOS Sensor Interface (CSI)] of the i.MX6 SL Reference Manual.

In particular - sections  16.1 (Overview) and 16.4 (Principles of Operation).

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SLRM.pdf


As for hardware specs, please the i.MX6 SL Datasheet, section 4.10.2
[CMOS Sensor Interface (CSI) Timing Parameters]

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SLCEC.pdf

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信