i.MX6 sololite parallel camera specifications

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 sololite parallel camera specifications

Jump to solution
1,968 Views
JHY
Contributor IV

I have a question about CSI camera parallel interface.

I want to know specifications or limitation of CSI of i.MX6 sololite.

Please let me know where the reference webs or documets are.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,615 Views
Yuri
NXP Employee
NXP Employee

  Please refer to Chapter 16 [CMOS Sensor Interface (CSI)] of the i.MX6 SL Reference Manual.

In particular - sections  16.1 (Overview) and 16.4 (Principles of Operation).

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SLRM.pdf


As for hardware specs, please the i.MX6 SL Datasheet, section 4.10.2
[CMOS Sensor Interface (CSI) Timing Parameters]

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SLCEC.pdf

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,616 Views
Yuri
NXP Employee
NXP Employee

  Please refer to Chapter 16 [CMOS Sensor Interface (CSI)] of the i.MX6 SL Reference Manual.

In particular - sections  16.1 (Overview) and 16.4 (Principles of Operation).

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SLRM.pdf


As for hardware specs, please the i.MX6 SL Datasheet, section 4.10.2
[CMOS Sensor Interface (CSI) Timing Parameters]

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SLCEC.pdf

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply