i.MX6 secure-boot can't enter Android system.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 secure-boot can't enter Android system.

1,681 Views
aresshsiao
Contributor II

I use android_M6.0.1_2.0.0_source BSP to develop my product.

 

Android: android-6.0.1_r22

Kernel: Linux/arm 4.1.15

The kernel config file is ".config"

The log message is "log2.txt"

In this enviornment, linux kernel will run to dead.

 

When I use "Linux/arm 3.14.52 Kernel" will no this problem.

Original Attachment has been moved to: .config.zip

Original Attachment has been moved to: log2.txt.zip

Labels (2)
0 Kudos
Reply
4 Replies

1,523 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aress

there are no specific errors related to security, so this may be

caused by build or programming issues. Please try fresh build

and program using MFG Tools

http://www.nxp.com/webapp/Download?colCode=IMX6_M6.0.1_2.0.0_MFG_TOOL&appType=license&location=null&... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,523 Views
aresshsiao
Contributor II

Hi Igor,

  I have two board, one is unburned secure-boot in CPU, another one is burned secure-boot in CPU. Then,  unburned secure-boot in CPU is can success work, the log file is "log1.txt", another log file is "log2.txt".

log1.txt

log2.txt

0 Kudos
Reply

1,523 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aress

unfortunately there is no such support for Android secure boot as for LInux,

suggest to elevate this through local fae channel.

Best regards
igor

0 Kudos
Reply

1,523 Views
aresshsiao
Contributor II

Hi Igor,

   Thanks for your reply and suggestion. I will retry another way.

Best regards,

Aress.

0 Kudos
Reply