i.MX6 secure-boot can't enter Android system.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 secure-boot can't enter Android system.

2,374 次查看
aresshsiao
Contributor II

I use android_M6.0.1_2.0.0_source BSP to develop my product.

 

Android: android-6.0.1_r22

Kernel: Linux/arm 4.1.15

The kernel config file is ".config"

The log message is "log2.txt"

In this enviornment, linux kernel will run to dead.

 

When I use "Linux/arm 3.14.52 Kernel" will no this problem.

Original Attachment has been moved to: .config.zip

Original Attachment has been moved to: log2.txt.zip

标签 (2)
0 项奖励
回复
4 回复数

2,216 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Aress

there are no specific errors related to security, so this may be

caused by build or programming issues. Please try fresh build

and program using MFG Tools

http://www.nxp.com/webapp/Download?colCode=IMX6_M6.0.1_2.0.0_MFG_TOOL&appType=license&location=null&... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,216 次查看
aresshsiao
Contributor II

Hi Igor,

  I have two board, one is unburned secure-boot in CPU, another one is burned secure-boot in CPU. Then,  unburned secure-boot in CPU is can success work, the log file is "log1.txt", another log file is "log2.txt".

log1.txt

log2.txt

0 项奖励
回复

2,216 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Aress

unfortunately there is no such support for Android secure boot as for LInux,

suggest to elevate this through local fae channel.

Best regards
igor

0 项奖励
回复

2,216 次查看
aresshsiao
Contributor II

Hi Igor,

   Thanks for your reply and suggestion. I will retry another way.

Best regards,

Aress.

0 项奖励
回复