i.MX6 sdk installing problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 sdk installing problem

1,601件の閲覧回数
michaelliang
Contributor I

Hi,

Firstly I have built a sdk for yocto. when I running the install script, it can't set it up. But this sdk can be install sucessfully in my European colleague's computer. Do I miss something to set up my system? Thank you!

 

160357_160357.jpg1.jpg

 

160358_160358.jpg2.jpg

Original Attachment has been moved to: ymer_sdk_log.zip

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,483件の閲覧回数
b36401
NXP Employee
NXP Employee

From the log I see that installation script unpacks /opt/ymer-fb/2.0.1 and than something inside is missing.
So first please check if you have enough disk space.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,483件の閲覧回数
michaelliang
Contributor I

I think the disk space is enough. I have uploaded the sdk to the cloud driver: http://pan.baidu.com/s/1c24xBcW

Thank you!

below is the disk information.

ming@ming-VirtualBox:~$ df -h
Filesystem Size Used Avail Use% Mounted on
udev 487M 4.0K 486M 1% /dev
tmpfs 100M 944K 99M 1% /run
/dev/sda1 177G 19G 149G 11% /
none 4.0K 0 4.0K 0% /sys/fs/cgroup
none 5.0M 0 5.0M 0% /run/lock
none 497M 152K 497M 1% /run/shm
none 100M 56K 100M 1% /run/user

0 件の賞賛
返信