i.MX6 - question about DDR memory bandwidth utilization

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 - question about DDR memory bandwidth utilization

2,095 次查看
marcin
Contributor I

Hi All,

Our board has i.MX6DL with 32@400MHz DDR3 modules. The memory has a 800 Mb/s per pin, which gives 3200 MB/s. Of course this is theoretical value only, but based on http://www.xilinx.com/support/documentation/white_papers/wp383_Achieving_High_Performance_DDR3.pdf, page 6, Table 1, bandwidth efficiency (clock_cycles_transferring_data / total_clock_cycles * 100) can vary (for optimized memory controller) between 57 % - 90 %.

The problem is that based on values from i.MX MMDC profiling mechanism, we can't get efficiency larger than 50 %.  I found that Francisco Dominguez in thread https://community.freescale.com/message/328259#328259, also wrote about 50 % of efficiency. The question is why?

The second question is about changing way of DDR connection from x32 to x64. What is real improvement in bandwidth? I think that double a bandwidth is not possible. Most of AXI masters are 64-bit, so improvement is possible only due to use of upsizers in NIC-301, am I right?

Thanks,

Marcin

标签 (1)
1 回复

1,277 次查看
Yuri
NXP Employee
NXP Employee

  Theoretical memory bandwidth calculations, assuming that data are provided at
every clock edge, are very "theoretical". Real DDR data access burst needs some
preparation stage : bus arbitration, RAS phase, CAS phase,CAS Latency and only
after that we can get data  at every clock edge. Comparing 64-bit and 32-bit performance,

only the recent stage (data  at every clock edge) provides some improvement.

0 项奖励
回复