i.MX6 pad control register; Speed field

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 pad control register; Speed field

1,280 次查看
stephanmeyer-lo
Contributor I

Hi all,

I have some issues using an SD-card below 0°C. (Every once in a while I don't read back what I wrote before). I solved the problem by changing the SPEED setting of the SD2_CLK from '01' (MEDIUM) to '00' (LOW). now everything works fine, but I can't see any changes using a scope.

Can anybody explain what the speed field in the pad_ctl_register does?

Kind regards

Stephan

0 项奖励
回复
2 回复数

1,037 次查看
saurabh206
Senior Contributor III

Hi,

Send your post to imx community (e.g. i.MX Community ) to get it visible for active members.

Saurabh

0 项奖励
回复

1,037 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Stephan

Those bits affect the slew rate control function within the IO cell,

allow for reducing switching noise. During board simulation, the various slew rates

should be simulated and the best one for the function of the signal should be selected for use.

'Low frequency" selection reduces noise and power consumption while signal latencies 

increased and vice versa.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复