i.MX6: gpu API glTexDirectVIVMap HSYNC abnormal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6: gpu API glTexDirectVIVMap HSYNC abnormal

4,431件の閲覧回数
linya
Contributor II

I update texture by glTexDirectVIVMap, there may be tearing on screen.
I check the message from


https://community.nxp.com/message/340399
https://community.nxp.com/message/812933
https://community.nxp.com/message/604667
https://community.nxp.com/message/614844

I test kernel version 3.14.28 and 3.14.52 with different number of FB-buffers.
bellow are my test result:

kernel=3.14.28 FB_MULTI_BUFFER=1 HSYNC abnormal
kernel=3.14.28 FB_MULTI_BUFFER=2 HSYNC ok
kernel=3.14.28 FB_MULTI_BUFFER=3 HSYNC ok

kernel=3.14.52 FB_MULTI_BUFFER=1 HSYNC abnormal
kernel=3.14.52 FB_MULTI_BUFFER=2 HSYNC abnormal
kernel=3.14.52 FB_MULTI_BUFFER=3 HSYNC ok

It's seems the GPU performance is turn to bad while upgrade it's version to
v5.0.11p7.4.

The question is : Why the new GPU version need one more buffer to solve the HSYNC problem?
One more buffer mean bad frame delay.
How to solve this problem with FB_MULTI_BUFFER=2 on new GPU version?

ラベル(3)
タグ(1)
7 返答(返信)

4,003件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi lin,

Latest BSP has GPU v5.0.11p8.6 that refine multi-buffer swap work flow on FB. You should try it.

fsl-arm-yocto-bsp.git - i.MX Linux BSP Release Yocto Project manifests 

regards

0 件の賞賛
返信

4,004件の閲覧回数
linya
Contributor II

Hi Bio_TICFSL

Could you disclose more detailed inside the multi-buffer swap work flow ?

0 件の賞賛
返信

4,004件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi lin,

The eglSwapInterval will work only when you enable multibuffering. Before starting the application

export FB_MULTI_BUFFER=2. This will make the EGL to use multibuffering and then try the eglSwapInterval. It will work.

Regards

0 件の賞賛
返信

4,004件の閲覧回数
linya
Contributor II

Hi Bio_TICFSL

I update BSP 3.14.52 with GPU v5.0.11p8.4 but  the problems still exist.  

I am not able to find the branch with GPU v5.0.11p8.6 from your git repertory.

Could you tell me the branch name?

regards

0 件の賞賛
返信

4,004件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi linya‌

It Refers to BSP version 4.1.15_2.0.0

regards

0 件の賞賛
返信

4,004件の閲覧回数
linya
Contributor II

Hi Bio_TICFSL

Thank you for your information.

I want to checkout BSP branch with 4.1.15_2.0.0  but failure.

$ ./repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1.15-2.0.0

fatal: Couldn't find remote ref refs/heads/imx-4.1.15-2.0.0

Then I try this:

$ ./repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1-krogoth

mv .repo/manifests/imx-4.1.15-2.0.0.xml .repo/manifests/default.xml

./repo sync

source and bitbake core-image

Check the gpu version on kernel. It's still GPU v5.0.11p8.4 instead of GPU v5.0.11p8.6

I also try this:

git clone git://git.freescale.com/imx/linux-imx.git

git branch -a

origin/imx_3.10.17_1.0.0_ga
origin/imx_3.10.53_1.1.0_ga
origin/imx_3.14.28_1.0.0_ga
origin/imx_3.14.52_1.1.0_ga
origin/imx_4.1.15_1.0.0_ga
origin/imx_4.1.15_2.0.0_ga
origin/imx_4.1.30_7ulp_alpha
origin/scm-imx_4.1.15_2.0.0_ga

I check gpu version on branch scm-imx_4.1.15_2.0.0_ga,  The version still  v5.0.11p8.4

finally I try this :

git clone git://git.freescale.com/imx/fsl-arm-yocto-bsp.git

git branch -a

master
remotes/origin/imx-3.10.17-1.0.0_ga
remotes/origin/imx-3.10.17-1.0.1_ga
remotes/origin/imx-3.10.17-1.0.2_ga
remotes/origin/imx-3.10.17-1.0.3_patch
remotes/origin/imx-3.10.53-1.1.0_ga
remotes/origin/imx-3.10.53-1.1.1_patch
remotes/origin/imx-3.10.53-1.1.2_patch
remotes/origin/imx-3.14.28-1.0.0_ga
remotes/origin/imx-3.14.28-1.0.1_patch
remotes/origin/imx-3.14.28-7D_alpha
remotes/origin/imx-3.14.38-6QP_beta
remotes/origin/imx-3.14.38-6QP_ga
remotes/origin/imx-3.14.38-6UL7D_beta
remotes/origin/imx-3.14.38-6UL_ga
remotes/origin/imx-3.14.38-6UL_patch
remotes/origin/imx-3.14.52-1.1.0_ga
remotes/origin/imx-4.1-krogoth
remotes/origin/imx-4.1.15-1.0.0_agl-demo
remotes/origin/imx-4.1.15-1.0.0_ga
remotes/origin/imx-4.1.15-1.0.0_genivi-demo
remotes/origin/imx-4.1.15-1.0.0_iotg-demo
remotes/origin/imx-4.1.15-1.0.0_xbmc-demo
remotes/origin/scm-imx-3.14.52-1.1.0_ga
remotes/origin/scm-imx-3.14.52-1.1.1_ga

There are no any branch named imx_4.1.15_2.0.0 or similar.

0 件の賞賛
返信

4,004件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi lin

L4.1.15_2.0.0 can be downloaded from NXP website:

Your costumer have some problem fetching the latest Yocto version, they can download it directly from nxp website:
or
Regards
0 件の賞賛
返信