i.MX6 dual processor sleep mode for android OS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 dual processor sleep mode for android OS

1,238 Views
farooqwaheed
Contributor I

Hi guys,

We are using i.MX6 dual processor for our project. We are using Android OS, we are running into some sleep mode issues. Our hardware team who build the board, tells us that we cannot implement a sleep mode, can we get some help to fill the knowledge gap so we can move forward with the project. I am the project manager and I am looking some high level information so I can assist my hardware team.

Thanks in advance

0 Kudos
Reply
1 Reply

1,205 Views
igorpadykov
NXP Employee
NXP Employee

Hi farooq

one can check Linux Manual (android is based on linux) and description of

low power drivers in Linux Documentation on link
i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply