i.MX6 boot from SPI-NOR Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 boot from SPI-NOR Flash

1,603 Views
JHY
Contributor IV

How I can write image to flash devices to boot from SPI-NOR?

Connecting the board to PC through USB-OTG port and using mfgtools can write to SPI-NOR, is it all right?

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

933 Views
igorpadykov
NXP Employee
NXP Employee

Hi conan

yes, it is right.

Please use Sabre-AI scheamtic, BSP and Linux Docs,

this board support booting from SPI-NOR.

i.MX6_SABRE_AI_DESIGNFILES

L3.0.35_4.1.0_LINUX_DOCS

SABRE for Automotive Infotainment Based on th|Freescale

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply