i.MX6 availabe PCIE memory access

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 availabe PCIE memory access

1,912件の閲覧回数
torus1000
Contributor V

Hi all,

Regard to PCIe of L3.14.28 Yocto i.MX6Q SabreSD BSP, I'm confusing now.

*  I believe i.MX6 support PCIe RC mode only so far.

*  According to the release note, there is PCIe EP/RC validation system.

*  I found a patch here:

      https://community.freescale.com/docs/DOC-95014

      https://community.freescale.com/message/544463

*  This system realized following features, I think.

      EP can access the memory of RC.

      RC can access the memory of EP.

Let me confirm some use cases as following, after patch applied;

(Q1)  Can FPGA(EP mode) access the  16MB memory of iMX6(RC mode)?

(Q2)  Can iMX6(RC mode) access the 256MB memory of FPGA(EP mode)?

(Q3)  Can iMX6(EP mode) access the 256MB memory of FPGA(RC mode)?

(Q4)  Can FPGA(RC mode) access the  16MB memory of iMX6(EP mode)?

I hope at least fist 2 answers are YES and BSP already supported them.

Can anyone help me?

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,434件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

please refer to link below describing BARs limit for memory regions

Re: PCIe BAR length limit

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,434件の閲覧回数
stjepanhenc
Contributor I

I know that Q2 works on Linux freescale 3.0.35 and i.MX6 Solo ARM processor.

0 件の賞賛
返信