Configuring 16-line RGB interface of I.MX6D for 16-bit LCD display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuring 16-line RGB interface of I.MX6D for 16-bit LCD display

1,257 Views
pramir
Contributor I

Hi All,

We want to know the configure details for 16-line RGB interface of I.MX6D for 16-bit LCD display.

Going through the below community forum,

https://community.freescale.com/thread/327695

we understand the below settings are required to send the RGB565 data over the DISP_DAT0 - DISP0_DAT15 in addition to VSYNC, HSYNC, PCLK.

  1. Timing in mxc_lcdif.c:

static struct fb_videomode lcdif_modedb[] = { 

  { 

     "320x240", 60, 240, 320, KHZ2PICOS(25000), 5, 5, 2, 2, 5, 2, 

     FB_SYNC_CLK_LAT_FALL, 

     FB_VMODE_NONINTERLACED, 

     0, 

  }, 

//... 

   2.   FB configuration in board-mx6dl_xxxx.c:

static struct fsl_mxc_lcd_platform_data lcdif_data = { 

  .ipu_id = 0, 

  .disp_id = 0, 

  .default_ifmt = IPU_PIX_FMT_RGB565, 

}; 

 

//... 

 

static struct ipuv3_fb_platform_data RIoTboard_fb_data[] = { 

  { 

  .disp_dev = "lcd", 

  .interface_pix_fmt = IPU_PIX_FMT_RGB565, 

  .mode_str = "320x240", 

  .default_bpp = 16, 

  .int_clk = false, 

  }, 

//... 

}

3.   Pin Muxing in board-mx6dl_xxxx.h:

/* DISPLAY */ 

MX6DL_PAD_DI0_DISP_CLK__IPU1_DI0_DISP_CLK, 

MX6DL_PAD_DI0_PIN15__IPU1_DI0_PIN15, /* DE */ 

MX6DL_PAD_DI0_PIN2__IPU1_DI0_PIN2, /* HSync */ 

MX6DL_PAD_DI0_PIN3__IPU1_DI0_PIN3, /* VSync */ 

//MX6DL_PAD_DI0_PIN4__IPU1_DI0_PIN4, /* Contrast not connected*/ 

MX6DL_PAD_DISP0_DAT0__IPU1_DISP0_DAT_0,

MX6DL_PAD_DISP0_DAT1__IPU1_DISP0_DAT_1,

MX6DL_PAD_DISP0_DAT2__IPU1_DISP0_DAT_2,

MX6DL_PAD_DISP0_DAT3__IPU1_DISP0_DAT_3,

MX6DL_PAD_DISP0_DAT4__IPU1_DISP0_DAT_4,

MX6DL_PAD_DISP0_DAT5__IPU1_DISP0_DAT_5,

MX6DL_PAD_DISP0_DAT6__IPU1_DISP0_DAT_6,

MX6DL_PAD_DISP0_DAT7__IPU1_DISP0_DAT_7,

MX6DL_PAD_DISP0_DAT8__IPU1_DISP0_DAT_8,

MX6DL_PAD_DISP0_DAT9__IPU1_DISP0_DAT_9,

MX6DL_PAD_DISP0_DAT10__IPU1_DISP0_DAT_10, 

MX6DL_PAD_DISP0_DAT11__IPU1_DISP0_DAT_11, 

MX6DL_PAD_DISP0_DAT12__IPU1_DISP0_DAT_12, 

MX6DL_PAD_DISP0_DAT13__IPU1_DISP0_DAT_13, 

MX6DL_PAD_DISP0_DAT14__IPU1_DISP0_DAT_14, 

MX6DL_PAD_DISP0_DAT15__IPU1_DISP0_DAT_15

Where,

DISP0_DAT0:DISP0_DAT4 - R0-R4

DISP0_DAT5:DISP0_DAT10 - G0-G5

DISP0_DAT11:DISP0_DAT15 - B0-B4

Please clarify if the above settings is enough to configure framebuffer (e.g. dev/fb0) as 320x240 16bpp (RGB565) and get the IPU to output the data 16-bits at a time.

Is there any other settings required to configure the internal DI format for data and commands for 16bits words such that the IPU driver outputs all LCD data in one clock over DISP0_DAT0:DISP0_DAT15.

Thanks & regards, Pramir

Labels (5)
Tags (1)
0 Kudos
3 Replies

901 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pramir

yes these settings are enough, in general process is well described in

sect.17.2 Adding Support for an LCD Panel i.MX53 System Development User’s Guide (rev.1, 3/2011)

http://www.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

901 Views
pramir
Contributor I

HI igor,

thanks for your reply.

In the figure 17-2 Interface, it shows that you have connected 18-data lines with display.

Since my display has only 16-data lines, could you confirm the below connections with display,

            DISP0_DAT0:DISP0_DAT4 - R0-R4

DISP0_DAT5:DISP0_DAT10 - G0-G5

DISP0_DAT11:DISP0_DAT15 - B0-B4

Thanks, Pramir

0 Kudos

901 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pramir

lcd mapping is given in datasheet

1.jpg

i.MX6DQ Datasheet (rev.4, 7/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards

igor

0 Kudos