i.MX6 android_jb4.2.2_1.1.0-ga make error (.../gcm/.../src': No such file or directory)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 android_jb4.2.2_1.1.0-ga make error (.../gcm/.../src': No such file or directory)

4,530 Views
tftu
Contributor III

Dear All:

     Have successfully make imx-android-13.4.1 (Android 4.0.4) on the exact same host without problem, but I got below error while switching to android_jb4.2.2_1.1.0-ga:

============================================

PLATFORM_VERSION_CODENAME=REL

PLATFORM_VERSION=4.2.2

TARGET_PRODUCT=sabresd_6dq

TARGET_BUILD_VARIANT=user

TARGET_BUILD_TYPE=release

TARGET_BUILD_APPS=

TARGET_ARCH=arm

TARGET_ARCH_VARIANT=armv7-a-neon

HOST_ARCH=x86

HOST_OS=linux

HOST_OS_EXTRA=Linux-3.5.0-28-generic-x86_64-with-Ubuntu-12.10-quantal

HOST_BUILD_TYPE=release

BUILD_ID=1.1.0-rc3

OUT_DIR=out

============================================

build/core/base_rules.mk:525: external/mtd-utils/new-utils/Android.mk: Module "ubinize" has useless module tags: eng. It will be installed anyway.

find: ‘../../vendor/unbundled_google/libs/gcm/gcm-client/src’: No such file or directory

find: ‘../../vendor/unbundled_google/libs/gcm/gcm-server/src’: No such file or directory

find: ‘../../vendor/unbundled_google/libs/gcm/gcm-client/src’: No such file or directory

find: ‘../../vendor/unbundled_google/libs/gcm/gcm-server/src’: No such file or directory

find: ‘src’: No such file or directory

PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/Effect_Tick.ogg:system/media/audio/ui/Effect_Tick.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/KeypressStandard.ogg:system/media/audio/ui/KeypressStandard.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/KeypressSpacebar.ogg:system/media/audio/ui/KeypressSpacebar.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/KeypressDelete.ogg:system/media/audio/ui/KeypressDelete.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/KeypressReturn.ogg:system/media/audio/ui/KeypressReturn.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/VideoRecord.ogg:system/media/audio/ui/VideoRecord.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/camera_click.ogg:system/media/audio/ui/camera_click.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/LowBattery.ogg:system/media/audio/ui/LowBattery.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/Dock.ogg:system/media/audio/ui/Dock.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/Undock.ogg:system/media/audio/ui/Undock.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/Lock.ogg:system/media/audio/ui/Lock.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/Unlock.ogg:system/media/audio/ui/Unlock.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/ringtones/ogg/Sceptrum.ogg:system/media/audio/ringtones/Sceptrum.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/KeypressStandard_120.ogg:system/media/audio/ui/KeypressStandard.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/KeypressSpacebar_120.ogg:system/media/audio/ui/KeypressSpacebar.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/KeypressDelete_120.ogg:system/media/audio/ui/KeypressDelete.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/KeypressReturn_120.ogg:system/media/audio/ui/KeypressReturn.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/notifications/ogg/Capella.ogg:system/media/audio/notifications/Capella.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/notifications/ogg/CetiAlpha.ogg:system/media/audio/notifications/CetiAlpha.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/notifications/ogg/Polaris.ogg:system/media/audio/notifications/Polaris.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/notifications/ogg/Pollux.ogg:system/media/audio/notifications/Pollux.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/notifications/ogg/Procyon.ogg:system/media/audio/notifications/Procyon.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/ringtones/ogg/Aquila.ogg:system/media/audio/ringtones/Aquila.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/ringtones/ogg/ArgoNavis.ogg:system/media/audio/ringtones/ArgoNavis.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/ringtones/ogg/Carina.ogg:system/media/audio/ringtones/Carina.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/ringtones/ogg/Centaurus.ogg:system/media/audio/ringtones/Centaurus.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/ringtones/ogg/Cygnus.ogg:system/media/audio/ringtones/Cygnus.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/ringtones/ogg/Draco.ogg:system/media/audio/ringtones/Draco.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/ringtones/ogg/Machina.ogg:system/media/audio/ringtones/Machina.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/ringtones/ogg/Orion.ogg:system/media/audio/ringtones/Orion.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/ringtones/ogg/Pegasus.ogg:system/media/audio/ringtones/Pegasus.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/ringtones/ogg/Pyxis.ogg:system/media/audio/ringtones/Pyxis.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/ringtones/ogg/Rigel.ogg:system/media/audio/ringtones/Rigel.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/ringtones/ogg/Scarabaeus.ogg:system/media/audio/ringtones/Scarabaeus.ogg ignored.

PRODUCT_COPY_FILES frameworks/base/data/sounds/ringtones/ogg/Solarium.ogg:system/media/audio/ringtones/Solarium.ogg ignored.

build/core/Makefile:32: warning: overriding commands for target `out/target/product/sabresd_6dq/system/etc/permissions/android.software.live_wallpaper.xml'

build/core/base_rules.mk:502: warning: ignoring old commands for target `out/target/product/sabresd_6dq/system/etc/permissions/android.software.live_wallpaper.xml'

No private recovery resources for TARGET_DEVICE sabresd_6dq

make -C kernel_imx -j4 uImage ARCH=arm CROSS_COMPILE=`pwd`/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi-

make[1]: Entering directory `/home/tftu/myandroid4.2.2/kernel_imx'

  CHK     include/linux/version.h

  CHK     include/generated/utsrelease.h

make[2]: `include/generated/mach-types.h' is up to date.

  CALL    scripts/checksyscalls.sh

  CHK     include/generated/compile.h

  Kernel: arch/arm/boot/Image is ready

  SHIPPED arch/arm/boot/compressed/lib1funcs.S

  AS      arch/arm/boot/compressed/lib1funcs.o

  LD      arch/arm/boot/compressed/vmlinux

  OBJCOPY arch/arm/boot/zImage

  Kernel: arch/arm/boot/zImage is ready

  UIMAGE  arch/arm/boot/uImage

Image Name:   Linux-3.0.35-06126-g0f2d6ad

Created:      Mon Aug 19 18:25:12 2013

Image Type:   ARM Linux Kernel Image (uncompressed)

Data Size:    4712128 Bytes = 4601.69 kB = 4.49 MB

Load Address: 10008000

Entry Point:  10008000

  Image arch/arm/boot/uImage is ready

make[1]: Leaving directory `/home/tftu/myandroid4.2.2/kernel_imx'

install -D kernel_imx/arch/arm/boot/uImage  out/target/product/sabresd_6dq/uImage

install -D kernel_imx/arch/arm/boot/zImage  out/target/product/sabresd_6dq/kernel

host Executable: mkfs.ubifs (out/host/linux-x86/obj/EXECUTABLES/mkfs.ubifs_intermediates/mkfs.ubifs)

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/libz.so when searching for -lz

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/libz.a when searching for -lz

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/liblzo2.so when searching for -llzo2

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/liblzo2.a when searching for -llzo2

/usr/bin/ld: cannot find -llzo2

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/libuuid.so when searching for -luuid

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/libuuid.a when searching for -luuid

/usr/bin/ld: cannot find -luuid

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/libm.so when searching for -lm

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/libm.a when searching for -lm

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/libc.so when searching for -lc

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/libc.a when searching for -lc

collect2: ld returned 1 exit status

make: *** [out/host/linux-x86/obj/EXECUTABLES/mkfs.ubifs_intermediates/mkfs.ubifs] Error 1

       Still got no clue to figure it out, highly appreciated to any suggestion or comment!

-tftu

0 Kudos
Reply
4 Replies

1,860 Views
rickchu
Contributor IV

All you can reference with Android build error with -llzo2 and -luuid on 64 bits ubuntu to find the solution with this issue.

0 Kudos
Reply

1,860 Views
angelarobinson
Contributor I

I have this same problem. What was the solution? I'm building on Ubuntu 11.04 64-bit and followed the instructions for creating the build environment. Everything seemed to install per the instructions.

0 Kudos
Reply

1,860 Views
varsmolta
Contributor V

seems like the build process is calling the native ld instead of the cross-compiler ld tool. Did you call the envSetup script in your terminal before invoking the build?

0 Kudos
Reply

1,860 Views
4guin4g4
Contributor IV

Hi,

Jelly bean can only be installed in a 64 bit Linux.. What versin of Ubuntu is your host PC running?