i.MX6: Yocto with OpenCL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6: Yocto with OpenCL

2,228 次查看
concerned12345
Contributor III

I have a Yocto build with core-image-minimal and I'd like to be able to add OpenCL. I do not want Qt or any image with Qt since this will bloat my image. I've already tried the following while keeping core-image-minimal:

https://community.nxp.com/thread/446633

https://community.nxp.com/thread/428397

After building I do not have any RPM package for OpenCL or any of its libraries as stated in the above threads. It seems the only way to add this is to create an image with Qt (i.e. fsl-image-qt5).

Is there a way to add OpenCL with the Vivante drivers to core-image-minimal so I can keep my image as small as possible?

0 项奖励
回复
1 回复

1,630 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

please look on

OpenCL Hello World 

White Paper on get started with OpenCL on iMX6.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复