Hi,
We are using imx6Q custom platform for our development which is based on sabresd platform.
We are using Linux 3.14.28_1.0.0-GA BSP for our development.
Our primary display is connected with LVDS0. The pixel format is RGB24 and bpp is 24. Here we are able to get the yocto GUI properly.
Then we tried to dump a raw picture (cat red.raw > /dev/fb0) on the display. But the LCD is not displaying the exact image.
We found that the Yocto GUI changes the display format to 16bpp. Please find the fbset values in below and the bpp is set to 16bpp here.
fbset
mode "1024x768-53"
# D: 56.883 MHz, H: 42.324 kHz, V: 52.511 Hz
geometry 1024 768 1024 768 16
timings 17580 160 24 29 3 136 6
rgba 5/11,6/5,5/0,0/0
endmode
Later, we have forced the display bpp into 24 bpp by below command. In this case, the Yocto GUI is not proper but the raw picture is proper format.
fbset -fb /dev/fb0 -depth 24
We want the Yocto GUI in 24bpp format so that we can dump the raw picture in proper format and proper Yocto GUI in 24bpp.
Please suggest us.
Thank You,
Regards,
Ansari