i.MX6 VPU Encoding

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 VPU Encoding

1,656件の閲覧回数
javiergrande
Contributor I

Dear all,

Do you know how long does it takes to encode a 1080p frame in iMX6 from input memory to output memory buffer in H.264 (about 8Mbps of bitrate)?

Is there some kind of example code to use as quick start setup?

Thanks.

Regards

Javier

ラベル(3)
1 返信

1,372件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Javier

I am not aware of such data, for testing one can use VPU examples in

i.MX 6Series Platform SDK : Bare-metal SDK

or ltib imx-test package, mxc_vpu_test L3.0.35_4.1.0_ER_SOURCE_BSP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------