i.MX6 TW6869 driver source code for Linux L4.1.15

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 TW6869 driver source code for Linux L4.1.15

1,863件の閲覧回数
waynekuo
Contributor III

Hi everyone,

Do NXP provide the driver source code of TW6869 on Linux L4.1.15?

I found a community thread provide the patch for L3.10.53 and L3.14.48.

How to pass DMA buffers from a Driver thru GStreamer 'v4l2src' plugin to Freescale IPU/VPU plugins 

Does these patches works on L4.1.15?

How can I get the source code of TW6869?

Any information / suggestion is helpful. Thank you.

Best Regrds,

Wayne Kuo

0 件の賞賛
返信
1 返信

1,325件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Wayne

sorry it is not supported in official nxp bsps, supported drivers can be

found in documentation (Release Notes) on link

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...


================================================================
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信