i.MX6 Solo support I2C and Ethernet interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 Solo support I2C and Ethernet interface

1,556 次查看
Ritul
Contributor I

Hello,

We are looking for i.MX6 Solo processor (single core cortex A9) to support I2C x 4 and Ethernet (100Mbps/1Gbps).

We found that there is contradictory observation while processor selection.

1. At NXP website in buy/parametrics option,  When selecting I2C x 4 and Ethernet 1Gbps x 1 there is no processor part suggested (refer - capture3 image).

2. In the pin config tool of nxp (P/N: MCIMX6S6AVM08AC) or datasheet, I2C x 4 and Ethernet (RGMII- 1Gbps or ENET/MII - 100Mbps) pins are available to define without conflict. (refer - capture5 image).

3. Not found pin muxing oMCIMX6S6AVM10AD in pin config. tool. (refer - capture4 image).

Please confirm that i.MX6 Solo (P/N: MCIMX6S6AVM10AD or  MCIMX6S6AVM08AC) shall support ethernet and I2C interfaces. If not, Kindly suggest the best suitable part no.

Thanks & Regards,

Ritul

标签 (2)
标记 (1)
0 项奖励
回复
0 回复数