i.MX6 Solo Lite boot from eMMC fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Solo Lite boot from eMMC fail

1,392 Views
m_c
Senior Contributor I

Customer found boot from eMMC fail and has two diagrams for boot okay and fail as below. In this design, only XTAL 24MHz is used and no RTC_XTAL. Is this fail because of ERR007927?

boot_success

boot_success.png

boot fail

boot_failure.png

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,231 Views
art
NXP Employee
NXP Employee

Yes, the effect of the ERR007927 erratum is the likely cause of the issue.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply