i.MX6 SDMA Reference Implementation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 SDMA Reference Implementation

Jump to solution
2,215 Views
haider
Contributor II

Greetings,

I am looking for a reference code for i.MX6 SDMA. If there is any source available please let me know.

It would be great if I can also get an example on how to use Serial with SDMA.

I already have Linux source, but I am looking for some kind of SDK or simpler version.

Thanks,

Haider

Labels (1)
1 Solution
1,734 Views
igorpadykov
NXP Employee
NXP Employee

Hi Haider

please refer to attached files and description in pdf file

Chapter 29 Configuring the SDMA Driver, full sdk can be obtained

creating service request.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,735 Views
igorpadykov
NXP Employee
NXP Employee

Hi Haider

please refer to attached files and description in pdf file

Chapter 29 Configuring the SDMA Driver, full sdk can be obtained

creating service request.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------