i.MX6 - SD3 WP problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 - SD3 WP problem

1,244 次查看
andyj25
Contributor I

Hi Everyone,

I'm trying to boot from an SD card, but I can only do it in "read-only" mode.

If I boot in "read-write" mode, it gives a kernel panic.

Bootargs for read-only:

setenv bootargs console=ttymxc0,115200n8 root=/dev/mmcblk1p2 ro rootwait rootfstype=ext4; mmc dev 2; fatload mmc 2:1 0x10800000 uImage; bootm 10800000

For read-write I use the same bootargs, just changing "ro" to "rw", and only then will it give a huge kernel panic.

Any suggestions?

-Andrew

标签 (1)
0 项奖励
回复
1 回复

1,120 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Is there a way to reproduce this in one of the freescale boards?

Can you provide more details of the changes you have done, etc.

Best Regards,

Alejandro

0 项奖励
回复