i.MX6 RGMII internal reference clock 125MHz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 RGMII internal reference clock 125MHz

Jump to solution
17,760 Views
neusch
Contributor II

I would use the internal clock for RGMII. The external Switch have no clock reference, because the 12 wire RGMII interface dont't support that.

configuration clock: (like Hardware Development Guide)

CCM_ANALOG_PLL_ENETn                        - 125MHz

ENET_CLK_SEL                                         - get enet tx reference clk from internal clock from anatop (loopback through pad), this clock also sent out to external PHY

IOMUXC_SW_MUX_CTL_PAD_GPIO16    - ENET_REF_CLK(signal)

It is possible to use ENET_REF_CLK(pad) then as GPIO ?    (IOMUXC_SW_MUX_CTL_PAD_ENET_REF_CLK)

I found this diskussion:

-------------------------------------------------------------------------------------------

iMX6 RGMII + ENET_REF_CLK/ENET_TX_CLK

FrankLiu        21.05.2013 19:54        

In RGMII Mode, only the pin "ENET_REF_CLK" could used as 125M reference clock input.

The 125M reference clock could be from PHY chip, or external oscillator, and could also be routed from GPIO_16(need software configuration).     also?

In RMII Mode, only two pins "GPIO_16" and "RGMII_TX_CTL" could be used as the 50M reference clock. The clock source could be from external oscillator or internal PLL, need software configuration. Please refer the document "I.MX6 Hardware Development Guide", Chapter 11

--------------------------------------------------------------------------------------------

It is possible to use the internal PLL 125MHz for RGMII without external PHY or external oscillator ?

So the workaround GPIO_16

it's confusing to me

Labels (1)
1 Solution
12,195 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Mathias,

Not sure if I understand your question. The i.MX6 processor doesn't have an internal ENET PHY, it only has the controller. You have to place an external PHY connected to this controller so your system is RGMII capable. Now, about the clock, the processor needs a 125MHz one at the ENET_REF_CLK pin. This can come from an external oscillator or from the processor's GPIO16 pin, but this GPIO has to be connected to the ENET_REF_CLK pin externally, there's no way to take the signal from there inside the processor.

Please let me know if I misunderstood anything or if you need anything else.

Best regards.

Jorge.

View solution in original post

0 Kudos
Reply
5 Replies
12,196 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Mathias,

Not sure if I understand your question. The i.MX6 processor doesn't have an internal ENET PHY, it only has the controller. You have to place an external PHY connected to this controller so your system is RGMII capable. Now, about the clock, the processor needs a 125MHz one at the ENET_REF_CLK pin. This can come from an external oscillator or from the processor's GPIO16 pin, but this GPIO has to be connected to the ENET_REF_CLK pin externally, there's no way to take the signal from there inside the processor.

Please let me know if I misunderstood anything or if you need anything else.

Best regards.

Jorge.

0 Kudos
Reply
12,195 Views
dank1
Contributor II

I have connected the GPIO16 pin externally to the ENET_REF_CLK pin in order to use as 125MHz reference clock.

According to Freescale technical support (via my distributor) this is not supported.

If you say It is as you wrote above, how do I need to setup the GPIO16 and ENET_REF_CLK registers in the CPU to achieve this?

Register Name="IOMUXC_SW_MUX_CTL_PAD_GPIO16" Address="0x020E0248" Value="0x????????"

Register Name="IOMUXC_SW_PAD_CTL_PAD_GPIO16" Address="0x020E0618" Value="0x????????"

Register Name="IOMUXC_ENET_REF_CLK_SELECT_INPUT" Address="0x020E083C" Value="0x????????"

Register Name="IOMUXC_SW_MUX_CTL_PAD_ENET_REF_CLK" Address="0x020E01D4" Value="0x????????""

Register Name="IOMUXC_SW_PAD_CTL_PAD_ENET_REF_CLK" Address="0x020E04E8" Value="0x????????""

Thank you

0 Kudos
Reply
12,195 Views
neusch
Contributor II

Hello Jorge,

you understand the question correctly.

> iMX6 Hardware Development Guide "12.4.1 Using the GPIO_16 pin to generate the reference clock"

Well, is it not possible to use a Daisy Chain register like RMII (50MHz) , to take the signal from there inside the processor ?

....it would be easier, not to route a 125MHz clock.

> iMX6Q Reference Manual

Unbenannt.jpg

best regards

0 Kudos
Reply
12,195 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Mathias,

Unfortunately there's no way to route the 125MHz clock internally like it is the case for the 50MHz one. The 125MHz clock has to be output at the GPIO16 and then routed back to the ENET_REF_CLK.

Best regards.

Jorge.

12,195 Views
dariopennisi
Contributor I

Hi Jorge,

in my setup i would like to remove PHY crystal so i'm hoping to generate 25 MHz from GPIO16, route it to the PHY and then route back the 125MHz clock from this to the ENET_REF_CLK.

does this setup work?

in any case it seems to me there is quite some confusion on the reference manual as there are two different ENET_REF_CLK signals to be dealt with. one is thesignal that can go to GPIO16(pin R2)/RGMII_TX_CTL (pin C23), which as far as i understand can be the output from the internal PLL and/or the input to the phy in RMII mode while the other one, called ENET_REF_CLK (pin V22) is the reference clock for the RGMII... maybe it would be good to differentiate these names given they're different things...