i.MX6 Operating Frequency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 Operating Frequency

ソリューションへジャンプ
2,537件の閲覧回数
madhusoodanabai
Contributor II

Hi,

We are using i.MX6 quad processor (PCIMX6Q6AVT10AA) in our design. We are trying to operate the processor at 1GHz speed but we are able to achieve till 792MHz speed. What may be the reasons for processor not operating at higher frequencies ?

Regards,

Madhusoodana Bairy


ラベル(1)
1 解決策
2,165件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Have you apply the properly voltage for high frequency operation?

For details, please see the i.MX6Q datasheet (IMX6DQAEC.pdf)

Table 7. Operating Ranges.

元の投稿で解決策を見る

2 返答(返信)
2,166件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Have you apply the properly voltage for high frequency operation?

For details, please see the i.MX6Q datasheet (IMX6DQAEC.pdf)

Table 7. Operating Ranges.

2,165件の閲覧回数
madhusoodanabai
Contributor II

Hi,

Yes, we have applied 1.35V to the core as per processor datasheet. However, we have even tried with 1.2V to the core. Is there any other particular voltage that has to be given to the core for high frequency operation?

Thanks.

With Regards,

Madhusoodana Bairy

From: jimmychan

Sent: Monday, December 03, 2012 10:22 AM

To: Madhusoodana Bairy

Subject: Re: i.MX Community - i.MX6 Operating Frequency

i.MX6 Operating Frequency

created by jimmychan in i.MX Community - View the full discussion

0 件の賞賛
返信