i.MX6 NAND install unsuccessfully from custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 NAND install unsuccessfully from custom board

1,187 Views
miguelhortelano
Contributor II

I've successfully installed a Yocto Image on NAND from an SD using a Variscite evaluation board with an i.MX6 SOLO SOM
Now I'm trying to perform the same action from my custom board but, although I'm not seeing any error during the flash process, it fails to boot.

These are the steps followed to flash the bootloader:

./flash_erase /dev/mtd0 0 0
./kobs-ng init -x $MEDIA/$SPL_IMAGE --search_exponent=1 -v
./flash_erase /dev/mtd1 0 0 2
./nandwrite -p /dev/mtd1 $MEDIA/$UBOOT_IMAGE

While these are the steps for the kernel

./flash_erase /dev/mtd2 0 0 2> /dev/null
./nandwrite -p /dev/mtd2 $MEDIA/$KERNEL_IMAGE > /dev/null
./nandwrite -p /dev/mtd1 -s 0x1e0000 $MEDIA/$KERNEL_DTB > /dev/null


Where:


MEDIA=/opt/images/Yocto
SPL_IMAGE=SPL-nand
UBOOT_IMAGE=u-boot.img-nand
KERNEL_IMAGE=uImage
KERNEL_DTB=imx6dl-var-som-solo.dtb


The only difference I can appreciate executing these commands is running kobs-ng -version 1.3-

Notice the following differences:

PropertyEvaluation boardCustom board
ECC Strength84
Page Size in Bytes21102084
Block Mark Byte Offset19992018
Block Mark Bit Offset04
m_u32EccBlockNEccType42
m_u32EccBlock0EccType42
m_u32BadBlockMarkerByte19992018
m_u32BadBlockMarkerStartBit04

Why are these properties different if SOM is the same? Both, binaries and executables are the same aswell

Could these differences causes the issue?

FYI Running cat /proc/cpuinfo gets the same result in both boards

processor     : 0
model name     : ARMv7 Processor rev 10 (v7l)
BogoMIPS     : 3.00
Features     : half thumb fastmult vfp edsp neon vfpv3 tls vfpd32 
CPU implementer     : 0x41
CPU architecture: 7
CPU variant     : 0x2
CPU part     : 0xc09
CPU revision     : 10

Hardware     : Freescale i.MX6 Quad/DualLite (Device Tree)
Revision     : 0000
Serial          : 0000000000000000

As a first approach I could cross-compile latest kobs from here but I duno if somebody else faced this problem.

I've also read about this issue but it seems it's not the same problem.

Thks in advance

Labels (1)
0 Kudos
Reply
1 Reply

1,047 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we cannot help you since you are using a different board and bsp from the one that we provide. I highly recommend you to go with Verisite. They will help you with this problem. I apologize for the inconveniences this could give you.

Best Regards,

Diego.

0 Kudos
Reply