i.MX6 - Linux support for Rapid Spanning Tree Protocol?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 - Linux support for Rapid Spanning Tree Protocol?

1,681 次查看
davidriness
Contributor I

Hello -

I am trying to find out if the ethernet driver in the Linux/Yocto build includes support for RSTP (Rapid Spanning Tree Protocol).

If so, can you point me to documentation?

All I can find is reference to Marvell saying it is supported....

Thanks in advance!

标签 (3)
0 项奖励
回复
2 回复数

1,375 次查看
b36401
NXP Employee
NXP Employee

You can refer to section 3.9 "RTSP streaming playback"

of i.MX 6 Series Yocto Project Multimedia User's Guide.

You can get the document from this pack:

http://www.freescale.com/webapp/Download?colCode=L3.10.17_1.0.0_LINUX_DOCS&Parent_nodeId=13376994810...

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,375 次查看
phdm
Contributor III

Question was about RSTP (which stands for Rapid STP (which stands for Spanning Tree Protocol)), not about RTSP (which stands for Real Time Streaming Protocol).  Maybe time to switch to 5-letters acronym :smileyhappy: