i.MX6 LCD display problem: Projector Shadow display

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 LCD display problem: Projector Shadow display

1,683 次查看
guochancen
Contributor I

Hi all,

        Now I have made a project of Camera-Projection with i.MX6 quad, it can display now.

        However when display the real-time image from the camera, the early image will not clear until ~30 seconds,like following:

        1.I put a paper under the camera

IMG_20150317_170839.jpg

2. When I move the paper, the image is still display

IMG_20150317_170848.jpg

My projector parameters are as following:

QVGA

Description               Min          Type            Max     Unit

Horizontal total         344           400              488     Pixel

Horizontal active        -               320             -          Pixel

Horizontal blank         -               80               -         Pixel

Vertical total             251           300             2000    line

Vertical active            -              240             -          line

Vertical blank             -              60              -          line

My linux driver is:

/* 320x240 @ 120 Hz , pixel clk @ 14.4MHz */

const char *name;  "My_projector",

u32 refresh; 120,

u32 xres;  320,

u32 yres;  240,

u32 pixclock;  69444,

u32 left_margin; 20,

u32 right_margin;  59,

u32 upper_margin;  20,

u32 lower_margin;  39,

u32 hsync_len;  1,

u32 vsync_len;  1,

u32 sync;  0,

u32 vmode;  FB_VMODE_NONINTERLACED,

u32 flag;  0,

What's the problem? What should I do?

标记 (3)
0 项奖励
回复
3 回复数

1,482 次查看
jamesbone
NXP TechSupport
NXP TechSupport

For the settings seems ok your configuration but we need the datasheet for review pixel clock or the front and back porch,  I believe this is the problem.

0 项奖励
回复

1,482 次查看
guochancen
Contributor I

Hi, jamesbone.Thanks for your reply!

But we have signed a confidentiality agreement with the company, so I can only give you part of the datasheet.

This projector only support DE mode, and the datasheet doesn't have the front and back porch, all specification is as following(the picture is cut from the datasheet, not scaled):

QVGA

Description               Min          Type            Max     Unit

Horizontal total         344           400              488     Pixel

Horizontal active        -               320             -          Pixel

Horizontal blank         -               80               -         Pixel

Vertical total             251           300             2000    line

Vertical active            -              240             -          line

Vertical blank             -              60              -          line

Frame Rate              -               120             -           Hz

Pixel clock              -                14.4M           -          Hz

未命名.bmp

The parameters from top to bottom are : VSYN, HSYN, (The parameter on original datasheet is not clear too,I can't recognize it),DE, CLK, R[5:0], G[5:0], B[5:0]

未命名.bmp

0 项奖励
回复

1,482 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Seems correct your configuration, is the cable of the projector near to any electric source, that may cause  EMC or any other interference?

0 项奖励
回复