Hi community,
I have two questions about i.MX6SDL IPU display clock generation.
Please see my questions below.
[Q1]
Please see chapter 38.1.10.3 in IMX6SDLRM.
It says "The DI clock can be derived from IPU's clock (HSP_CLK) or from an external source (via the DIn_DISP_CLK - ipp_di_#_ext_clk pin)".
Next, please see chapter 38.5.194.
The discription explains about display clock generation only mede from HSP_CLK.
But I think I can generate display clock from external source by setting this field if I select external source by di0_clk_ext in chapter 38.5.193.
[Q2]
I want to confirm how to set the fractional part of dix_disp_clk_period in chapter 38.5.194.
I understand display clock will be" HSP_CLK / (1 + 1/16)" if I set dix_disp_clk_period = 0x011.
And it will be "HSP_CLK / (1+ 1/2)" if I set dix_disp_clk_period = 0x018.
Is my understanding correct?
Best Regards,
Satoshi Shimoda