i.MX6 GPU Timer deadlock, exit by timeout !!!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 GPU Timer deadlock, exit by timeout !!!

1,639 次查看
woogeunshin
Contributor II

Hi,

I'm using  i.MX6 dual core and its platform is Android 4.3.

Our board raises this error suddenly in the early morning. At that time, nobody uses the board. 

After this error, ANR occurred in the several applications.  Reason of ANR is "android.intent.action.TIME_TICK".

Other symptoms were LCD off, no event for Key press, no event for Touch LCD. It looks like deadlock.

To recover this problem, I have to power reboot.

I've never reported and seen this problem even though several thousand products are running on the sites.

This is the first time. So, I doubt that the device has physical fault.

If anybody has similar experience, please share opinion and experience.

I attached Kernel exception log.

Regards, 

Shin.

标签 (1)
0 项奖励
回复
1 回复

1,521 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Shin

Android 4.3 is very old release and since many gpu fixes were implemented

in latest releases, recommended to migrate to new Android releases found on

i.MX Software|NXP 

Support for old releases is provided through  NXP Professional Services:

NXP Professional Services|NXP 

General steps may be: apply JB_4.3_1.1.1_Patch as described in attached document and

upgrade to L3.0.101 kernel

https://www.nxp.com/webapp/Download?colCode=L3.0.101_4.1.1_SOURCE_BSP&appType=license&locati... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复