i.MX6 GPIO pull up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 GPIO pull up

Jump to solution
2,717 Views
sugiyamatoshihi
Contributor V

Hi,

I have a question pin output setting.

When a port is  output mode, it means OBE is enabled or functional output, is it possible to enable keeper or pull up/down resistor? 

In application note, AN5078, there is a description below.

The keeper device is able to keep the previous output value when the output driver is disabled.

Best Regards,

Sugiyama

Labels (2)
0 Kudos
Reply
1 Solution
2,455 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

I apologize, but I do not understand what you want to your question.  However, if you want to know if it is possible to enable/disable the keeper. Yes, it is possible.

Best Regards,

Diego.

View solution in original post

0 Kudos
Reply
2 Replies
2,456 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

I apologize, but I do not understand what you want to your question.  However, if you want to know if it is possible to enable/disable the keeper. Yes, it is possible.

Best Regards,

Diego.

0 Kudos
Reply
2,455 Views
sugiyamatoshihi
Contributor V

Hi, Diego,

Thank you for the answer.

I also think it is strange. I asked customer why pullup/down is required in output mode, but no answer, yet.

Anyway, I understand pullup/down  and keeper can enable regardless input and output mode.

Best Regards,

Sugiyama

0 Kudos
Reply