i.MX6 GPIO Slew Rate Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 GPIO Slew Rate Configuration

ソリューションへジャンプ
2,776件の閲覧回数
menghuaho
Contributor I

Hi,

Need help from fellow freescale community members with regards configuration of imx6D/Q GPIO output slew rate.

We are attempting to configure iMX6D/Q GPIO (GPIO6_IO08) to have a slew rate (green lines) to the region of around 600us. Currently, we are only able to configure to 4-5us slew rate (10%-90%, rising edge), using DSE via pad configuration.

Would it be possible to adjust PUE, PKE and pull-up resistance (100K) to achieve that too?

Appreciate if there would be some additional info/source examples for this.

Thanks for your help.

pastedImage_2.png

pastedImage_0.png

ラベル(1)
0 件の賞賛
返信
1 解決策
2,350件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Meng

one can try with settings :

SRE=0, SPEED=0, ODE=1 Output is Open Drain,

PKE=0, PUE=1, PUS=10 - 100K Ohm Pull Up

Also one can try to add capacitor for slope tweaking.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,350件の閲覧回数
menghuaho
Contributor I

Hi Igor,

Thanks and appreciate your advise on this matter.

This worked for me instead.

========================================

SRE=0, SPEED=0, ODE=1 Output is Open Drain,

PKE=1, PUE=1, PUS=10 - 100K Ohm Pull Up

============================================

Thanks again.

0 件の賞賛
返信
2,351件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Meng

one can try with settings :

SRE=0, SPEED=0, ODE=1 Output is Open Drain,

PKE=0, PUE=1, PUS=10 - 100K Ohm Pull Up

Also one can try to add capacitor for slope tweaking.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------