i.MX6 - Ethernet Multicast testing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 - Ethernet Multicast testing

2,547件の閲覧回数
Ansari
Contributor IV

Hi,

We are using imx6Q sabresd platform for our development with Linux 3.10.17_1.0.0-GA BSP.

We would like to test the Ethernet multicast testing in our target board.

Please let us know, what are the packages has to be included in the yocto file system.

In addition, please provide the steps to do the Ethernet multicast testing.

Thank You,

Regards,

Ansari

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,952件の閲覧回数
jamiew
Contributor III

Hi Ansari

Did you get multicast working? Whenever I try to send to udp video to 239.0.0.1 I get an error. However ifconfig shows MULTICAST on the i.mx

Thanks


Jamie

0 件の賞賛
返信

1,952件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

There is not a multicast demo or documentation for it specifically that I know of. That being said the Ethernet driver available as part of the BSP does support multicast. You can confirm if it’s enabled by looking at the information shown by ifconfig where you can see the flag MULTICAST if it’s enabled.

You may want to look at the code available on the i.MX6 SDK (link below) regarding Ethernet and RTP.

https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null&fasp=1&WT_TYPE=So...

There are some examples on the web on multicast that may be of help as well. You can even find some information from other users in our communities like in the link below:

https://community.freescale.com/message/267761#267761

Hopefully someone on the communities can share their experience with it.

0 件の賞賛
返信