Hello All!
Have i.MX 6Quad Freescale SabreSD with Android 4.3
I want to connect to SabreSD the wifi module RTL8723BS by SDIO.
The main problem is:
I configure everything according to the instructions, but unfortunately it is not going to build like a KO (module).
Step by step:
- vim kernel_imx/arch/arm/configs/imx6s_{yourdevice}_android_defconfig
CONFIG_CFG80211=y
CONFIG_MAC80211_MESH=y
CONFIG_MAC80211=y
CONFIG_HOSTAP=y
CONFIG_RTL8723BS=m
2. vim device/fsl/{yourdevice}/BoardConfig.mk
BOARD_WIFI_VENDOR := realtek
ifeq ($(BOARD_WIFI_VENDOR), realtek)
WPA_SUPPLICANT_VERSION := VER_0_8_X
BOARD_WPA_SUPPLICANT_DRIVER := NL80211
CONFIG_DRIVER_WEXT :=y
BOARD_WPA_SUPPLICANT_PRIVATE_LIB := lib_driver_cmd_rtl
BOARD_HOSTAPD_DRIVER := NL80211
BOARD_HOSTAPD_PRIVATE_LIB := lib_driver_cmd_rtl
BOARD_WLAN_DEVICE := rtl8723bs
WIFI_DRIVER_MODULE_NAME := "wlan"
WIFI_DRIVER_MODULE_PATH := "/system/lib/modules/wlan.ko"
WIFI_DRIVER_MODULE_ARG := "ifname=wlan0 if2name=p2p0"
WIFI_FIRMWARE_LOADER := ""
WIFI_DRIVER_FW_PATH_STA := ""
WIFI_DRIVER_FW_PATH_AP := ""
WIFI_DRIVER_FW_PATH_P2P := ""
WIFI_DRIVER_FW_PATH_PARAM := ""
endif
3. Add android.hardware.wifi.direct.xml
PRODUCT_COPY_FILES += \
frameworks/native/data/etc/android.hardware.wifi.direct.xml:system/etc/permissions/android.hard
ware.wifi.direct.xml
4. init.xxx.rc
service rtw_suppl_con /system/bin/wpa_supplicant \
-ip2p0 -Dnl80211 -c /data/misc/wifi/p2p_supplicant.conf -e/data/misc/wifi/entropy.bin -N \
-iwlan0 -Dnl80211 -c/data/misc/wifi/wpa_supplicant.conf
class main
socket wpa_wlan0 dgram 660 wifi wifi
disabled
oneshot
service rtw_suppl /system/bin/wpa_supplicant -iwlan0 -Dnl80211
-c/data/misc/wifi/wpa_supplicant.conf
socket wpa_wlan0 dgram 660 wifi wifi
class main
disabled
oneshot
5. Set wifi.interface
PRODUCT_PROPERTY_OVERRIDES += \
wifi.interface=wlan0
6. Apply wifi_realtek.c
ifeq ($(BOARD_WIFI_VENDOR), realtek)
LOCAL_SRC_FILES += ../realtek/wlan/libhardware_legacy/wifi/wifi_realtek.c
else
LOCAL_SRC_FILES += wifi/wifi.c
endif
7. wpa_supplicant_8
ifeq ($(BOARD_WIFI_VENDOR), realtek)
L_CFLAGS += -DREALTEK_WIFI_VENDOR
L_CFLAGS += -DANDROID_P2P
L_CFLAGS += -DCONFIG_ANDROID_4_2_PERSISTENT_IOT
Endif
8. Adding or Selecting Target Platform
opt/kernel_imx/drivers/net/wireless/rtl8723bs/makefile
CONFIG_PLATFORM_FSL_IMX6Q = y
CONFIG_PLATFORM_I386_PC = n
CONFIG_PLATFORM_ANDROID_X86 = n
CONFIG_PLATFORM_ARM_S3C2K4 = n
CONFIG_PLATFORM_ARM_PXA2XX = n
CONFIG_PLATFORM_ARM_S3C6K4 = n
CONFIG_PLATFORM_MIPS_RMI
= n
CONFIG_PLATFORM_RTD2880B
= n
CONFIG_PLATFORM_MIPS_AR9132 = n
CONFIG_PLATFORM_MT53XX
= n
CONFIG_PLATFORM_RTK_DMP
= n
9. opt/kernel_imx/drivers/net/wireless/Makefile
obj-$(CONFIG_RTL8723AS) += rtl8723as/
10. opt/kernel_imx/drivers/net/wireless/Kconfig
source "drivers/net/wireless/rtl8723bs/Kconfig"
The build is building success, but i don't get the KO module file in opt/out/target/product/sabresd_6dq/system/lib/module/
Thank's a lot for any help or ideas!