i.MX6 EIM burst write timing.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 EIM burst write timing.

Jump to solution
2,095 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 EIM.

Please see chapter 22.8.7 & 22.8.8 in IMX6DQRM (Rev.2).

I can see the burst read memory access timing diagram, but not find burst "write" memory access timing diagram.

Could you send me the burst write memory access timing diagram?

Best Regards,

Satoshi Shimoda

Labels (4)
Tags (1)
0 Kudos
Reply
1 Solution
1,580 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

write access is the same as read with one difference: asserted EIM_WE

[EIM_RW] signal. You can refer to Figure 15 "Synchronous Memory, Write Access"

IMX6DQCEC i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,581 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

write access is the same as read with one difference: asserted EIM_WE

[EIM_RW] signal. You can refer to Figure 15 "Synchronous Memory, Write Access"

IMX6DQCEC i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply