i.MX6 Dual RAM Supported?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 Dual RAM Supported?

ソリューションへジャンプ
2,575件の閲覧回数
rmstark
Contributor I

Hi Everyone,

I have a question about what RAM the MX6 Dual will support. I am looking to use part number: MCIMX6D7CVT08AD. 

In the reference design (which uses a QuadCore MX6Q) they call out Quantity 4: DDR3L 2Gb RAM at 800MHz to reach 1GB total.

In the combined datasheet for the Quad and Dual it says only DDR3-1066 and LPDDR2-1066 are supported (see attached printscreen). 

I'm having a hard time finding non-last time buy or obsolete RAM at 533MHz/1066 Data Rate. 

My question is, with the Dual model I've chosen can I use an 800MHz module such as the one below, or is there a functional difference that only allows the MX6Q to use 800MHz/1600 data rate RAM? 

Alliance Memory: AS4C512M16D3L-12BCN 

If this won't work can you suggest a 1GB (8Gb) module I could use that is active (in production)?

Thanks for your time and help. 

タグ(4)
1 解決策
2,451件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  it is possible to use the mentioned part with i.MX6.

http://www.alliancememory.com/pdf/ddr3/8GB-AS4C512M16D3L.pdf 

Please use the https://community.nxp.com/docs/DOC-94917 to configure the memory.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,452件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  it is possible to use the mentioned part with i.MX6.

http://www.alliancememory.com/pdf/ddr3/8GB-AS4C512M16D3L.pdf 

Please use the https://community.nxp.com/docs/DOC-94917 to configure the memory.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------