i.MX6 Development board with full parallel camera interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 Development board with full parallel camera interface

1,220 次查看
pascalrosin
Contributor I

Hi, I am looking for a development board, where all signals for the parallel camera interface of the i.MX6 are available.

We want to interface a camera with Y/Cb/Cr 4:2:2 BT.709 16-bit parallel interface to encode the 1080p30 image stream.

For development, an Ethernet port would be nice and maybe a USB host connector. Everything else is optional.

Can you suggest a development board?

Cheers

Pascal

标签 (2)
标记 (1)
0 项奖励
回复
1 回复

938 次查看
DavorBogavac
NXP Employee
NXP Employee

Hi Pascal,

There are no Freescale boards that I am aware of where you can do this. But there are many other board suppliers for the i.mx6.

Here are 2 examples.

https://www.toradex.com/products/freescale-i.mx6

i.MX6 Development kit | i.MX6 Reference Design | i.MX6 Development Board

Both have SOM + base board configurations that will enable you access to at least 1 CSI port with all 20 data pins.

Regards

Davor

Best Regards
Davor
0 项奖励
回复