i.MX6 DL support PCM digital audio interface?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 DL support PCM digital audio interface?

Jump to solution
2,224 Views
高丽哲
Contributor I

Our have a CDMA module which only support  PCM digital audio interface, could i.MX6 DL support PCM ? Could i use the SSI(I found it only support I2S and AC97 in reference ?) connect to CDMA module and how to configure it ?

thanks

0 Kudos
Reply
1 Solution
1,954 Views
igorpadykov
NXP Employee
NXP Employee

Hi 高 丽哲

some PCM modes may be supported, some not, since

term "PCM" is quite generic and wide, it can imply quite

different interfaces. I think you should check required timings waveforms

and check what is supported by i.MX6 audio interfaces

described in sect.61.8.1, 26.1.2 Modes of Operation  IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,247 Views
MaazPatni
Contributor II

CONFIG_SND_SOC_TLV320AIC32X4=y

CONFIG_SND_SOC_TLV320AIC32X4_I2C=y

To interface the TLV320AIC3204 with the i.MX8MP, it’s necessary to enable the driver of the CODEC in our defconfig file.

For more refer this Click Here

0 Kudos
Reply
1,955 Views
igorpadykov
NXP Employee
NXP Employee

Hi 高 丽哲

some PCM modes may be supported, some not, since

term "PCM" is quite generic and wide, it can imply quite

different interfaces. I think you should check required timings waveforms

and check what is supported by i.MX6 audio interfaces

described in sect.61.8.1, 26.1.2 Modes of Operation  IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply