i.MX6 DL support PCM digital audio interface?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 DL support PCM digital audio interface?

ソリューションへジャンプ
2,255件の閲覧回数
高丽哲
Contributor I

Our have a CDMA module which only support  PCM digital audio interface, could i.MX6 DL support PCM ? Could i use the SSI(I found it only support I2S and AC97 in reference ?) connect to CDMA module and how to configure it ?

thanks

0 件の賞賛
返信
1 解決策
1,985件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 高 丽哲

some PCM modes may be supported, some not, since

term "PCM" is quite generic and wide, it can imply quite

different interfaces. I think you should check required timings waveforms

and check what is supported by i.MX6 audio interfaces

described in sect.61.8.1, 26.1.2 Modes of Operation  IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,278件の閲覧回数
MaazPatni
Contributor II

CONFIG_SND_SOC_TLV320AIC32X4=y

CONFIG_SND_SOC_TLV320AIC32X4_I2C=y

To interface the TLV320AIC3204 with the i.MX8MP, it’s necessary to enable the driver of the CODEC in our defconfig file.

For more refer this Click Here

0 件の賞賛
返信
1,986件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 高 丽哲

some PCM modes may be supported, some not, since

term "PCM" is quite generic and wide, it can imply quite

different interfaces. I think you should check required timings waveforms

and check what is supported by i.MX6 audio interfaces

described in sect.61.8.1, 26.1.2 Modes of Operation  IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信