i.MX6 DDR3 Write leveling error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 DDR3 Write leveling error

4,584 次查看
sugiyamatoshihi
Contributor V

Hi, 

I have a question about write leveling error on DDR3 in Hardware Write Leveling Calibration.

There return HW_WL_ERR and during HW write leveling sometimes. It seems calibration stop first DQS calibration and then it didn't go through fine tune.

Are there suspicious to stop fine tune calibration? Do you have a any experience like this?

Attached picture are OK case and NG case.  Left picture is OK case and right picture is NG case.

Best Regards,

Sugiyama

标签 (1)
0 项奖励
回复
8 回复数

4,312 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  According to section 44.11.6.1 (Hardware Write Leveling Calibration)

of i.MX 6Dual/6Quad Applications Processor Reference Manual, Rev. 3, 07/2015 :

" ...

8. MMDC repeates steps 5-7 till the write leveling delay is 1 cycle

9. MMDC checks the 8 bit prime DQ results for each DQS and finds the first transition from 0 to 1.

    If no transition is found then the MMDC indicates an error at MPWLGCR[HW_WL_ERR#].

..."

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,313 次查看
sugiyamatoshihi
Contributor V

Hi, Yuri,

Thank you for the answer. 

However, according to waveform, there is one transition 0-1 in DQ at NG case, but error was set.

Do you think why this first transition couldn't found?

Should I check any other registers?

Best Regards,

Sugiyama

0 项奖励
回复

4,313 次查看
sugiyamatoshihi
Contributor V

Hi, Yuri,

Do you have any comment on this?

However, according to waveform, there is one transition 0-1 in DQ at NG case, but error was set.

Do you think why this first transition couldn't found?

Should I check any other registers?

Best Regards,

Sugiyama

0 项奖励
回复

4,313 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Since HW_WL_ERR is set - there was no any 0->1 transition found. in the NG case.

Regards,

Yuri.

0 项奖励
回复

4,313 次查看
sugiyamatoshihi
Contributor V

Hi, Yuri,

I'm sorry I missed the register bit in MMDCx_MPWLGCR.

There is no error bit in WL_HW_ERRx, but WL_SW_RES2 was set.

It seems HW recognize as the 0->1 transistion when DQ is high at the first DQS.

However, I couldn't understand why there is no 0->1 tansition during fine tune.

Best Regards,

Sugiyama

0 项奖励
回复

4,313 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Again : 

  As for the case, when  DQS is high at the first DQS in Write Leveling Calibration : this is not a problem, since  just edge  of 0->1 transition event is important. DQS will be delayed for the next steps till “0” with following “1” will be detected.

   In Your situation - perhaps - some glitches  (on prime DQ) occur, interpreted as 0->1 edge by the MMDC. Also, please check DRAM datasheet regarding Write Leveling Calibration, it may be, that additional settings of DRAM Mode Registers should be performed.

Regards,

Yuri.

0 项奖励
回复

4,313 次查看
sugiyamatoshihi
Contributor V

Hi, Yuri,

There are further question.

When calibration tool run, Write leveling and DQS delay results are below.  DQS2 delay is 0/256 ,

and WL_DL_ABS_OFFSET2 (Byte2) in MMDC_MPWLDECTRL1 is 0x00 in the data. Then it seems it related to write leveling error.

Start write leveling calibration...
running Write level HW calibration
Write leveling calibration completed, update the following registers in your initialization script
MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x0004000F
MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x00020000
Write DQS delay result:
Write DQS0 delay: 15/256 CK
Write DQS1 delay: 4/256 CK
Write DQS2 delay: 0/256 CK
Write DQS3 delay: 2/256 CK

What is supposed to cause by when this delays are 0?

Best Regards,

Sugiyama

0 项奖励
回复

4,313 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  You may try the recommended after calibration values and if test is OK - why do not use them ?

Regards,

Yuri.

0 项奖励
回复