i.MX6 Coin Cell Charge Current

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Coin Cell Charge Current

Jump to solution
3,466 Views
ko-hey
Senior Contributor II

Hi

I have a question about PMIC Coin Cell Charger Specifications.

MMPF0100.pdf has a flowing table.

coincell_current.PNG.png

Coin cell charge current in on mode ICOINHI is typically 60μA.

Is the number per second or hour?

Best Regards

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
3,217 Views
Yuri
NXP Employee
NXP Employee

  The Coin Cell Charge current is just 60 uA. It is applied to compensate

cell self discharge. The coin cell charger may be software enabled / disabled.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
3,218 Views
Yuri
NXP Employee
NXP Employee

  The Coin Cell Charge current is just 60 uA. It is applied to compensate

cell self discharge. The coin cell charger may be software enabled / disabled.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,217 Views
ko-hey
Senior Contributor II

Hi Yuri

Thank you for your reply.

However, unfortunately I think my intention is not transmitted.

I'll give you an actual example.

If I use a coin cell that has capacity of 6.5mAh, How long will it take to charge it?

In my understanding, the charger supplies 60uA of current per second.

So it will take 15-20 minutes.

Is this correct?

Best Regards,

0 Kudos
Reply
3,217 Views
Yuri
NXP Employee
NXP Employee

To fully charge, say 6.5 mA x hour  - it will take about 110 hours ( 6.5 mA x hour  / 60 uA ).

~Yuri.

3,217 Views
ko-hey
Senior Contributor II

Yuri

Thanks a lot!

ko-hey

0 Kudos
Reply
3,217 Views
ko-hey
Senior Contributor II

Dear Yuri

Sorry, I was misunderstood.

Please forget the above question.

ko-hey

0 Kudos
Reply