i.MX6 - Android and hardware-backed KeyStore

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 - Android and hardware-backed KeyStore

1,880 Views
andrzejdziedzic
Contributor IV

Hi,

is it possible to have a hardware-backed KeyStore in the i.MX6 device with Android M6.0.1_2.0.0?

What should be implemented to use i.MX6 security functions by the KeyStore Android API?

Best regards,

Andrzej Dziedzic

Labels (3)
0 Kudos
Reply
1 Reply

1,684 Views
Yuri
NXP Employee
NXP Employee

Hello,

  "As far as the trusty OS is concerned, NXP does not have hardware-backed Keystore implemented.

Thus currently the Software Keystore implementation by google can only be used.

However, Linaro has an implementation of the master key for android here

https://github.com/OP-TEE/optee_os/tree/kmgk_pta_3.3.0

  The safer approach for a pure android customer would be to go with trusty.

If one wants both a Linux and Android solution and want to keep compatibility between the 2, then it may

need to investigate optee."

Regards,

Yuri.

0 Kudos
Reply