i.MX6 Android UVC (USB Video Class)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 Android UVC (USB Video Class)

2,513件の閲覧回数
eishishibusawa
Contributor III

Customer has developed the system with android jb4.2.2_1.1.0-ga(from Freescale/NXP) on IMX6DualLite.

It can use the USB camera of UVC by using Android standard Camera API.

 

Q.

Is the following module related to UVC operation?

 

/device/fsl-proprietary/gpu-viv/lib/libg2d.so

 

Best Regards,

Eishi SHIBUSAWA

 

ラベル(2)
0 件の賞賛
返信
1 返信

2,045件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

this file has not direct relation to usb module operations, just for

reference please refer to sect.11.1.1.3 Source Code Structure

attached Linux Manual for L3.0.35 which is used in android jb4.2.2.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信