i.MX6 Android UVC (USB Video Class)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Android UVC (USB Video Class)

2,552 Views
eishishibusawa
Contributor III

Customer has developed the system with android jb4.2.2_1.1.0-ga(from Freescale/NXP) on IMX6DualLite.

It can use the USB camera of UVC by using Android standard Camera API.

 

Q.

Is the following module related to UVC operation?

 

/device/fsl-proprietary/gpu-viv/lib/libg2d.so

 

Best Regards,

Eishi SHIBUSAWA

 

Labels (2)
0 Kudos
Reply
1 Reply

2,084 Views
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

this file has not direct relation to usb module operations, just for

reference please refer to sect.11.1.1.3 Source Code Structure

attached Linux Manual for L3.0.35 which is used in android jb4.2.2.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply