i.MX6 Android UVC (USB Video Class)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 Android UVC (USB Video Class)

2,589 次查看
eishishibusawa
Contributor III

Customer has developed the system with android jb4.2.2_1.1.0-ga(from Freescale/NXP) on IMX6DualLite.

It can use the USB camera of UVC by using Android standard Camera API.

 

Q.

Is the following module related to UVC operation?

 

/device/fsl-proprietary/gpu-viv/lib/libg2d.so

 

Best Regards,

Eishi SHIBUSAWA

 

标签 (2)
0 项奖励
回复
1 回复

2,121 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

this file has not direct relation to usb module operations, just for

reference please refer to sect.11.1.1.3 Source Code Structure

attached Linux Manual for L3.0.35 which is used in android jb4.2.2.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复