i.MX6 Android Framebuffer Config for 16bit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 Android Framebuffer Config for 16bit

3,413件の閲覧回数
johnson_zhang
Contributor I

I use a i.MX6Q SabreSD to test the framebuffer.

I want to make a config that:

HDMI output @ 1280*720P - bpp=32bit

and a dummy output @ 480*800 - bpp=16bit(I only want to use the frame buffer content, to copy to outsie devices as projector ).

But whatever I config via command line or board***.c, the frame buffer color depth for the dummy device(ldb or lcd) always be 32bit(RGBA?)

How can I config it?

Best regards.

ラベル(3)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,549件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

would you show what command line you used? and what changes in the board***.c?

also, it is better to tell what BSP and board are you using.

thanks.

0 件の賞賛
返信

2,549件の閲覧回数
johnson_jl
Contributor I

Thanks Jimmy.

We use a SabreSD board, and try to set bpp=16 for HDMI/LCD display.

But seems that FB0/FB2 only use RGBA format for the UI display data.

What we want is try to copy RGB565 framebuffer data as treaming out, but seems Android 4.2.2 only use RGBA(32bit) for it's display device framebuffers.

Please help me check it.

0 件の賞賛
返信

2,549件の閲覧回数
varsmolta
Contributor V

Hi were you able to figure this out? I am also using android 4.2.2 build and 16-bit lcd and not getting anything on my lcd. I've tested my lcd using yocto linux so I know my init sequence for initializing the lcd is ok. My android boot params are:

enable_wait_mode=off console=ttymxc0,115200 vmalloc=400M consoleblank=0 rootdelay=3 video=mxcfb0:dev=lcd,DTECH,if=RGB666 video=mxcfb1:off video=mxcfb2:off fbmem=28M fbcon=28M androidboot.bootdev=sdhci-esdhc-imx.0 androidboot.hardware=freescale androidboot.console=ttymxc0

where DTECH is the name of my lcd and i've added this to mxc_lcdif as well.

Thanks

0 件の賞賛
返信