i.MX6 AUDMUX setting when TX <-> RX swapping.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 AUDMUX setting when TX <-> RX swapping.

ソリューションへジャンプ
2,531件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I havea a question about AUDMUX setting.

I understand the setting when not swapping TX and RX in How should I set i.MX6 AUDMUX_PTCR and AUDMUX_PDCR. .

Then, how about in the case of the attached file?

Best Regards,

Satoshi Shimoda

ラベル(4)
タグ(1)
0 件の賞賛
返信
1 解決策
2,347件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

connections in attached file are quite ambiguous as in

I.MX6 connection AUDMUX port 7 with SSI3 is internally fixed and

usual connection (device_TXD -> AUD_TXD, AUD_RXD->device_RXD)

does not require TXRXEN switch set.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,348件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

connections in attached file are quite ambiguous as in

I.MX6 connection AUDMUX port 7 with SSI3 is internally fixed and

usual connection (device_TXD -> AUD_TXD, AUD_RXD->device_RXD)

does not require TXRXEN switch set.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信