i.MX6 ASRC processing clock.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 ASRC processing clock.

Jump to solution
1,981 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a questions about i.MX6 ASRC processing clock.

Please see Table 15-1 in IMX6SDLRM Rev.1.

The foot note 2 says "FsASRC is the processing clock of ASRC block"

I want to confirm which clock is "the processing clock".

Which clock is "the processing clock" in Table 15-4 in IMX6SDLRM?

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
1,708 Views
Yuri
NXP Employee
NXP Employee

The processing clock is main / system module clock, for the ASRC it is SPDIF1_CLK_ROOT, please look at
Figure 18-3 (Clock Tree - Part 2) of the i.MX6 SDL RM.

View solution in original post

0 Kudos
Reply
1 Reply
1,709 Views
Yuri
NXP Employee
NXP Employee

The processing clock is main / system module clock, for the ASRC it is SPDIF1_CLK_ROOT, please look at
Figure 18-3 (Clock Tree - Part 2) of the i.MX6 SDL RM.

0 Kudos
Reply