i.MX6 ASRC processing clock.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 ASRC processing clock.

ソリューションへジャンプ
2,005件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a questions about i.MX6 ASRC processing clock.

Please see Table 15-1 in IMX6SDLRM Rev.1.

The foot note 2 says "FsASRC is the processing clock of ASRC block"

I want to confirm which clock is "the processing clock".

Which clock is "the processing clock" in Table 15-4 in IMX6SDLRM?

Best Regards,

Satoshi Shimoda

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
1,732件の閲覧回数
Yuri
NXP Employee
NXP Employee

The processing clock is main / system module clock, for the ASRC it is SPDIF1_CLK_ROOT, please look at
Figure 18-3 (Clock Tree - Part 2) of the i.MX6 SDL RM.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,733件の閲覧回数
Yuri
NXP Employee
NXP Employee

The processing clock is main / system module clock, for the ASRC it is SPDIF1_CLK_ROOT, please look at
Figure 18-3 (Clock Tree - Part 2) of the i.MX6 SDL RM.

0 件の賞賛
返信