i.MX6 ASRC_ASRCTR setting.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 ASRC_ASRCTR setting.

Jump to solution
2,347 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a questions about i.MX6 ASRC_ASRCTR setting.

Please see chapter 15.7.1 in IMX6SDLRM Rev.1.

I understand pair A will automatic update when ATSA bit is 1, and update manually by USRA and IDRA bit when ATSA bit is 0.

Then, how about when the following setting?

Pair A will automatic update? or ASRC internal measured ratio will be used?

ATSA = 1

USRA = 1

IDRA = 0

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
2,147 Views
Yuri
NXP Employee
NXP Employee

Pair A will automatic update, based on ASRC internal measured ratio.

View solution in original post

0 Kudos
Reply
3 Replies
2,148 Views
Yuri
NXP Employee
NXP Employee

Pair A will automatic update, based on ASRC internal measured ratio.

0 Kudos
Reply
2,146 Views
satoshishimoda
Senior Contributor I

Hi Yuri,

According to your reply, ATSA setting and {USRA, IDRA} setting are applied at the same time.

Then, how about {ATSA, USRA, IDRA} = {1,0,0}.

I guess USRA & IDRA is ignored and "Pair A will automatic update its pre-processing and post-processing options based on the frequencies it detected".

Is this correct?

Best Regards,

Satoshi Shimoda

0 Kudos
Reply
2,147 Views
satoshishimoda
Senior Contributor I

Can somebody reply me?

0 Kudos
Reply